1. Jul11

    Posted on Tuesday, July 11, 2017

    Supplying an AC/DC Power Supply from a DC source

    A frequently asked question concerns the suitability of using an AC/DC power supply with a DC source. There are two parts to the answer, one concerning the ability of the converter to run without issue and the other concerning the safety aspects.

    Read more

    Tags: AC/DC power supplies | View count: (551)

  2. Jul26

    Posted on Tuesday, July 26, 2016

    Robust 650 W supply meets MIL-STD-810F and ANSI/ISA standards for demanding applications

    The HHP650 series of rugged AC-DC power supplies are designed for heavy-use industrial applications where an electrically & mechanically robust solution is required.

    Read more

    Tags: AC/DC power supplies, Reliability | View count: (108)

  3. Sep29

    Posted on Tuesday, September 29, 2015

    Green mode LLC half bridge converters

    Power supplies marketed under the “Green” label are designed to maximise efficiency across the load range (average active mode efficiency) and minimise power consumed at no load. Active mode efficiency is the average of four measurements made at 25, 50, 75 & 100% of...

    Read more

    Tags: Green Power, AC/DC power supplies, Power Supply Topologies | View count: (83)