1. Jun13

    XP Power launches low profile 225 Watt power supply in compact 3”x5” U-channel format

    Posted on Tuesday, June 13, 2017

    UCP225

    XP Power has announced the UCP225 series of high power density, very low profile 225W AC/DC power supplies with both industrial and medical safety approvals in a small U-channel footprint.

    Read more

    Tags: Low Profile, High Power Density, AC-DC Power, AC-DC, U-Channel | View count: (2608)

  2. Oct12

    XP Power launches world’s smallest 40 Watt AC-DC open frame power supply

    Posted on Wednesday, October 12, 2016

    ECF40

    XP Power today announced the ECF40 series of single output 40 Watt ultra compact AC-DC power supplies. These open frame convection-cooled units are capable of delivering the full output power of 40 Watts without the need for any external forced air flow up to + 50 degrees C....

    Read more

    Tags: High Efficiency, Open-frame, Single Output, Medical, AC-DC | View count: (8090)

  3. Sep15

    XP Power launches digitally controlled 1U configurable power platform

    Posted on Thursday, September 15, 2016

    nanofleX

    XP Power today announced the nanofleX series of configurable digitally controlled AC-DC power supplies. This modular supply is constructed in a compact low profile 1U mechanical chassis format that suits today’s space constrained designs and can accommodate up to four...

    Read more

    Tags: Configurable, AC-DC | View count: (5153)

  4. Feb9

    Low profile IT and medical 90 Watt external power supplies comply with Level VI

    Posted on Tuesday, February 9, 2016

    AJM90

    XP Power today announced the AJM90 series of 90 Watt single output external AC-DC power supplies. Meeting the US Department of Energy’s new Level VI no load / standby power and active mode efficiency specification, the AJM90 consumes less than 0.21 Watt when no load is...

    Read more

    Tags: Medical, External/Desktop, AC-DC | View count: (8408)