Selecting power supplies for peak load applications
Specifying an AC/DC power supply for systems with peak load requirements that are higher than the normal power requirements for short periods can result in larger, higher power and higher cost product selection.
In these applications the average power required is typically significantly lower than the peak demand and, with care, savings in product size and cost can be realized without compromising system reliability or lifetime. Using a power supply that can support the peak load but with a lower continuous power rating will result in a physically smaller power supply reducing system size, weight and cost. The supply must be electrically rated to safely support the peak demand but can be thermally rated at the lower power level.
Applications that require higher peak currents typically include electromechanical elements such as print heads, pumps, motors, and drives. These products are found in factory automation, medical devices, fluid & material handling, robotics, power tools, machining, packaging, test, dispensing systems and printers and have average power demands far lower than the peak power requirements
Some products specify a peak load capability which can be characterized in a number of different ways.
The power supply is rated for up to 30s with a duty cycle of 10 to 15% at a peak load that is just below the Over Current Protection (OCP) limit.
The OCP is usually set around 20 to 30% above the continuous current rating. This is essentially a standard design, evaluated and characterized to give short duration headroom over and above the nominal continuous rating. Taking advantage of these characteristics to support peak power demands results in a smaller lower cost supply provided that the average power demand is below the maximum continuous rating.
A higher power rating at high-line, normally meaning 180 VAC and above.
A 1200W power supply may be able to provide 1500W of continuous power when operated at an AC line voltage greater than 180 VAC. This is a genuine size and cost benefit if the AC input is in the high line range and is ideal for higher power systems connected from phase to phase when the nominal single-phase supply is low.
A power supply with the topology and thermal characteristics, designed to support high peak electromechanical loads.
Such units may deliver up to twice their nominal power for 10 seconds or more with duty cycles up to 35% for demanding electromechanical applications in industrial process control. XP’s fleXPower modular power system is one example which allows several standard outputs alongside one that provides a high peak current.
Dual rated power supplies
Often overlooked when considering peak load applications are power supplies with a convection rating and a higher fan cooled rating. It is not uncommon for such a supply to be rated at up to 50% higher power when fan cooled compared to a naturally cooled environment.
Such products are naturally electrically rated for the higher power rating and thermally rated for the convection cooled power rating. These are the exact characteristics we need for peak load applications where the peak load is does not exceed the fan cooled rating and the average load is lower than the convection rating, without the noise nuisance of a cooling fan.
In general, the larger the difference between the fan cooled rating and the convection rating the shorter the peak load capability and it is important to ensure that components do not overheat during peak load periods. A benefit for the system designer is that these dual rated products will normally identify key components and their temperature ratings to ensure safe and reliable operation when installed in end applications. This information can be used to ensure that the product will remain safe and reliable in a peak load application by monitoring the temperature of the key parts during the development phase.
The specification will also typically outline the lifetime expectations based on key electrolytic capacitor temperatures enabling confirmation of the suitability of the product based on system requirements.
When selecting such a power supply for a high peak power application the key parameters are the peak power required, which must not exceed the fan cooled rating, the maximum duration of the peak, the duty cycle and power consumed by the load during the non-peak duration to ensure that the continuous convection ratings of the supply are not exceeded.
The following example is based on an open frame power supply with a force cooled rating of 250W and a convection or naturally cooled rating of 180W, XP Power’s GCS250 series, operating in a convection cooled application where the system requires a peak load of 250W for 10s in every 40s or a duty cycle of 25%.
This peak load (Ppk) requirement defines the absolute maximum power consumption during the non-peak period so that the average power does not exceed the convection cooled rating.
In this case, the maximum available power during the non-peak duration (Po) will be 156 Watts in order that the convection cooled power rating (Pav) is not exceeded.
Pav = (Ppk x T1) + (Po x T2)
T1 +T2
Using the same formula, if the duty cycle is reduced 15%, or 10s in every 67s then the non-peak power can be increased to 168W without exceeding the average continuous convection power rating of 180W.
Calculations show that these operating conditions will not exceed the ratings of the power supply. However, as previously highlighted, we must also consider the key component temperatures of the supply when installed in the unique end equipment to ensure safe, reliable operation over the design life of the end equipment.
The diagrams below show the maximum temperature of the components for this product to ensure that the safety and reliability requirements are met and the predicted service life of the product based on the average capacitor operating temperature over the life of the equipment can be realized.
In order to ensure safe operation of the PSU in the end-use equipment, the temperature of the components listed in the table below must not be exceeded. The temperature should be monitored using K type thermocouples placed on the hottest part of the component (out of direct air flow). See mechanical details for component locations.
Selecting and evaluating a product such as this, based on the readily available thermal data, rather than one continuously rated for the full peak power results in a smaller, lighter, lower cost solution without compromising the performance, reliability and lifetime of the end application.