Articles techniques - Haute Tension

Next-Generation, Miniature High Voltage Power Modules

The first generation of high voltage power modules changed the way designers could use high voltage, and the next-generation is pushing the envelope further.

Minimizing the Impact of Source Resistance on High-Voltage DC to DC Converters

A primer for systems designers

Application Note - Input Bypass Capacitor

This Application Note describes the optional use of an input bypass capacitor for improved performance.

Application Note - Connecting Proportional Models for Positive or Negative Outputs

This Application Note describes how to connect proportional models for either positive or negative output.

Application Note - How to Connect and Test a Proportional Model

This Application Note details how to connect and test an proportional model to verify operation.

Application Note - Proportional No Load Variation

This Application Note describes operation of high voltage proportional converters with varying load conditions.

Application Note - How to Connect and Test a Regulated Model

This Application Note describes how to connect and test a regulated unit.

Application Note - Reverse Polarity Protection

This Application Note describes how to protect a high voltage supply from a negative input voltage. A negative input voltage may cause damage to the unit.

Application Note - High Voltage and Load Current Monitors

This Application Note describes how high voltage and load current monitors work with all high voltage products.

Application Note - Design Considerations for the Q Series

This Application Note describes all the necessary considerations when designing in a Q Series product.