XP Power - power supplies
  1. Feb5

    Posted on Tuesday, February 5, 2019

    Selecting power supplies for peak load applications

    Specifying an AC/DC power supply for systems with peak load requirements that are higher than the normal power requirements for short periods can result in larger, higher power and higher cost product selection. In these applications the average power required is typically...

    Read more

    Tags: Medical, AC/DC power supplies, power supplies, factory automation | View count: (1195)

  2. Dec3

    Posted on Monday, December 3, 2018

    IEC 62368-1, EN 62368-1 & UL 62368-1 Approved Power Supplies & DC-DC Converters

    The New Safety Standard for ITE and AV Equipment IEC/EN/UL 62368-1 is the new safety standard with a broad scope that covers ITE, communication technology, audio/video & similar type of equipment. It is a convergence of safety standards to replace IEC 60950 & IEC 60065 as...

    Read more

    Tags: DC-DC Converter, 62368-1, safety standard, power supplies, HSBE | View count: (2234)

Archive