1. Sep7

    Posted on Thursday, September 7, 2017

    MIL-STD-1275  Compliance for power systems made easy.

    The US Department of Defense Standard MIL-STD 1275 is an immunity standard that defines a series of test conditions to be applied to the input of a 28V electrical power system within a military vehicle.  These include spikes, surges, operating voltages and ripple

    Read more

    Tags: Defence | View count: (672)

  2. Feb21

    Posted on Tuesday, February 21, 2017

    DEF-STAN 61-5 Part 6, Issue 6, Compliance Made Easy

    In February 2009, the UK Ministry of Defence published issue 6 of Defence Standard 61-5 part 6 to cover 12 and 24V systems. This issue 6 version has a major change when compared to issue 5 which had been originally published in 1990. The main difference is to define how electrical...

    Read more

    Tags: Defence | View count: (258)

  3. May26

    Posted on Thursday, May 26, 2016

    Active surge protection filter module complies with DEF STAN 61-5 issue 6 load dump requirement

    The DSF226 EMC filter and surge protection module is designed for use in 28 VDC input defense applications. The PCB mounting module is encapsulated within a six sided metal enclosure and is able to support up to 200 Watts output power to drive downstream DC-DC converters.

    Read more

    Tags: DC-DC Converter, Defence | View count: (160)