• Power supplies designed for healthcare,
    industrial and technology applications
Powering the World's Critical Systems

Product Selector Tool

Whether it’s AC-DC or DC-DC, our product selector has everything you need to find the perfect power supply or converter for your application.

App Download

Our product selector tool is also available as a free downloadable app. Choose from the iOS or Android version by clicking on the link below.

Sample Request

Power supply sample units are available free of charge for qualifying applications. Follow the link below to request your sample.

Brochures & Catalogs

We have a wide range of literature to help you choose the right product. Literature is available in both downloadable and paper copy formats upon request.

Latest Product News

Stock Check

Custom Power Supplies

Custom power supplies provide cost effective solutions where applications cannot be fulfilled from our standard product range or where integrated products are required.

Product Image
Energy efficiency for external power supplies (EPS)
Gary Bocock
/ Categories: Blog, RSS

Energy efficiency for external power supplies (EPS)


image

Energy efficiency legislation is now in place across most regions of the world. In the main, the focus of these regulations is on the operating efficiency and the no-load “standby” power consumption of external power supplies. Driven by the proliferation of external power supply products and the environmental impact of leaving power supplies always turned on despite the load not being in use, most legislation set limits for what is considered to be a viable no-load consumption. Being better able to control and lower the power consumed by external power supplies, whether a load is connected or not, helps to deliver a significant reduction in the environmental impact. 

In the USA there are a number of bodies legislating on energy efficiency; the California Energy Commission (CEC), US Congress with its Energy Independence and Security Act (EISA) and recently the United States Department of Energy (DoE). There is also Energy Star that sets limits for electrical and electronic equipment.

In Europe, there is the Energy related Products (ErP) Directive formerly known as the Energy Using Products (EuP) directive, which is mandatory. There is also the EU Code of Conduct for external power supplies that is voluntary.

In Canada, there is Natural Resources Canada (NRCan) and in Australia the Minimum Energy Performance Standard (MEPS). 

These are just a few examples of mandatory requirements written into legislation.

Recently both the US DoE and the EU CoC have updated their energy efficiency standards. These changes apply to both the no-load energy consumption limit and that of the typical operating energy efficiency. At the same time the EU CoC has also added an energy efficiency requirement intended for those applications where, for most of its operating time, the load consumes a relatively small amount of power from the external power supply. Initially requiring a power supply to meet an efficiency target at a 10% load requirement, the new standard has two tiers intended to assist in defining new developments. 

The DoE and EU CoC were both introduced in early 2014 with both the DoE and EU CoC tier 2 requirements coming into force in 2016. These new requirements mean both increased active mode efficiency and reduced no-load power consumption. The tables below outline the differences between the level IV and level V limits previously invoked the new DoE level VI limits and the EU CoC tier 1 & tier 2 limits with implementation dates. Notably, the DoE limits now incorporate external power supplies with an output power greater than 250W. Devices that require Federal approval as a medical device are exempt from the DoE legislation.


table
table
table
table
table

Delivering energy efficient appliances to the market has become a key marketing requirement. Energy tariffs have increased significantly over the past years and together with increasing energy awareness, consumers and business buyers alike have energy efficiency as a key selection criterion.
External power supplies with both Level VI and CoC tier 2 energy efficiency ratings are readily available, including those with medical safety approvals, as market demands lead legislation.


Previous Article MIL-STD-1275 Compliance for power systems made easy.
Next Article Reliability Terminology
Print
400 Rate this article:
5.0

Please login or register to post comments.